Part Number: TL072
Hi,
The attached circuit is designed for a power supply of 9 volts, and the power supply of the class D amplifier, TPA3251D2 is 26 volts. Can I use 26 volts without conversion (down to 9 volts) to power the preamp with some changes to the circuit? The microphone, that will be connected to the preamp has an impedance of 200 ohms. Is it matched to the input of the preamp? Can I replace POT1 with a digital potentiometer without significant changes in the circuit? Please also for a quick check of the circuit, because I am not familiar in depth with the audio circuitry.
Best regards,
Tsvetan