This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OPA615: Fast Bipolar Peak Detector

Part Number: OPA615

Hi team,

My customer found a problem using OPA615IDR. The schematic diagram of OPA615IDR is as follows:

When OPA615_IN network is suspended, after ± 5V voltage is applied, some OPA615 chips can measure about 45mv DC level on ADC network. In my opinion, under normal circumstances, when pin10 of OPA615 is input 0V, Pin2 output 0V is normal. Is that right ?

Cross experiment: the chip on the normal board is welded to the abnormal board, and the abnormal board becomes normal; the chip removed from the abnormal board is welded on the normal board, and the normal board becomes abnormal. The chip was purchased on TI store. Is this caused by chip differences? Could you give any suggestions

  • Hello Amy,

    I don't believe the offset at the emitter should be as high as it is, however there is also no input offset voltage spec for the SOTA in the datasheet. Would you be able to measure the voltages at pins 10 & 11 & 2 of both normal and abnormal devices?

    Best,

    Hasan Babiker

  • Hi Hasan Babiker,

    Thanks for your response.  The voltage of each pin is shown in the table below

    OPA615 pins value

    normal

    abnormal

    Pin2

    0mV

    42mV

    Pin3

    0mV

    42mV

    Pin4

    107mV

    -4.24V

    Pin5

    -4.88V

    -4.88V

    Pin10

    0mV

    0mV

    Pin11

    0mV

    42mV

    ADC network

    0mV

    42mV

  • Hi Amy,

    I'm sorry, but this circuit makes no sense to me:

    amy_opa615.TSC

    What is the purpose of this circuit?

    Kai

  • Hello Amy,

    Surprised to see that pin 4 is being driven down to -4.24V for pin 4, device maybe damaged. Is this the only unit that is showing this type of response?

    Best,

    Hasan Babiker 

  • Hi Kai,

    Thanks for your response.

    But the customer feedback said that this circuit test is OK, the following is the customer test waveform

    Because when the input of this circuit is 0, the output is about 40 ~ 200mV DC level, so the circuit can only detect the peak voltage of input > 200mV

  • Hello Hasan,

    The customer tested a total of nine chips, five of which were abnormal.

    What is the cause? Is the circuit designed correctly? Will soldering cause this problem

  • Hi Amy,

    something is wrong in the schematic you showed in the original post. Why are there two Schottky diodes, U309 and D303, in parallel? And how shall this circuit be able to perform a bipolar peak detection? Even if only an unipolar peak detection is desired the circuit as shown in the schematic will not work because another Schottky diode to signal ground is missing.

    Can you please show an updated schematic? :-)

    Kai

  • Hello Amy,

    I agree the parallel diodes here isn't clear to me as well. There was also an addition of a 1k-ohm resistor for R321 that isn't in the "Fast Bipolar Peak Detector" circuit in the OPA615 datasheet.

    Best,

    Hasan Babiker

  • Hi Amy,

    the scope plots show a rather low frequency of about 50kHz. In this frequency range a peak detector using standard OPAmps might be a better choice :-)

    What is the customer wanting to do? Can you elaborate a bit, please?

    Kai