This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi there,
is it possible to use this or another IC for "DCR current sensing" over an inductor after a half bridge? Something like this:
"TPS65311-Q1 BUCK1 Controller DCR Current Sensing" (SLVA791)
it's a little bit like peak current sensing, only for better unterstanding.
We already have a digital controller, so we only need the signal.
Best regards
Marcel
Marcel,
I will need to look at the document as I am not familiar with it but just skimming through it. The thing I worry about it the AC CMRR and Bandwidth with respect to input voltage and the negative recovery when Vsense <0. I have attached snap shots of the spots in the datasheet.
For AC CMRR you can see the CM input to the Device is like a step function meaning it has high frequency components.
Bandwidth-The bandwidth is not constant with your input Vsense and this could cause issues as the switch is going from low to high current. This is less and an issue as the inductor should have current during the times of concerns but realize the bandwidth does change.
Vsense <0. This could be a transient and could place the device in a state that can cause issues as the input of Vsense can temprarly can go below Zero.
Hi Javier,
thanks for response. Yeah you are right. Unidirectional is the value I missed. But INA240 is bidirectional? And it's also quite fast with 400 kHz.
What do you think?
Best regards
Marcel
Hello Marcel,
I believe that would be a better option and it has the PWM rejection which will help with the switching conditions.
Regards,