This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

INA281-Q1: Does INA281-Q1 support bidirectional current sensing?

Part Number: INA281-Q1

Hi team,

My customers is considering using INA281-Q1 as their current sensing solution to sense a bidirectional current to/from a 12V battery. As my understanding, since the input range is at least from -6V to 6V for INA281-Q1. It should be supporting the bidirectional current sensing with proper selection of the shunt resistor? Am I understanding this correctly? 

I just write this thread in order to confirm and remove the concern from my customers since the bidirectional current sensing is not written in the datasheet.

BR,

Manu