This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi All,
I have a question about OPA541AP.
When used with RCL = 0.2Ω, I think ILIM will be about + 3.3A.
As a result of evaluation on the customer's board, it was 2.3A
Also, the output voltage and output current are decreasing.
Will it be within the guaranteed operation range?
I understand that ± 10% fluctuates due to the inflow of output current.
I also understand that the output current fluctuates depending on the temperature.
How much semiconductor variation does the device have?
Best Regards,
Ishiwata
Ishiwata-san,
The OPA541 is one of our earlier power op amp developments and the current limit function is not precise. You may notice that there are not any current limit specifications listed in the Electrical Characteristics table. The actual current limit of a particular device will be a function of its transistor base-emitter voltages (VBE) and the external current limit resistor accuracy and its behaviors.
Both the temperature dependent transistor VBE and current limit resistor's accuracy and temperature coefficient affect the point where limiting occurs. Figure 8. the Current Limit vs Resistance Limit vs Temperature graph gives some idea just how much the current limit range can be affected by temperature. Section 8.1.1, Current Limit, in the datasheet provides a good explanation of the current limit function and behavior.
If you need tighter current limit control and its other parameters meet your application's requirements the OPA549 uses a different, more predictable current limit design that is voltage reference based. The high output current does not flow through the current limit resistor decreasing circuit power dissipation, voltage drop, and the physical size of the resistor.
Regards, Thomas
Precision Amplifiers Applications Engineering