Hello,
I need to identify replacement op amps for the AD711, AD8627 and ADA4000-1 from ADI. What are the best P2P(Pin to Pin) replacement amplifiers from TI? Is OPA991 the best one for it?
Thanks!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
I need to identify replacement op amps for the AD711, AD8627 and ADA4000-1 from ADI. What are the best P2P(Pin to Pin) replacement amplifiers from TI? Is OPA991 the best one for it?
Thanks!
Hi Katherine,
You can look at our newest high voltage op amp OPA991, which is a 4.5MHz, single channel, low Vos and low noise amplifier. It’s RRIO and the slew rate is 21V/us.
Here is a table showing the performance differences among AD711, AD8627 and ADA4000-1, and the recommended device.
Thank you,
Tim Claycomb