Part Number: LM2903
Hi,
Could you please tell me the difference between LM2903D and LM2903VQDR?
Thank you so much for your help!
Best regards,
Wendy
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: LM2903
Hi,
Could you please tell me the difference between LM2903D and LM2903VQDR?
Thank you so much for your help!
Best regards,
Wendy
"V" indicates the enhanced voltage version (see the recommended operating conditions).
"Q" indicates that the device has been tested to automotive specifications.
"D" indicates the SOIC package.
"R" indicates tape&reel.
It is suggested to replace it with the LM2903BIDR.
One minor clarification..
A "Q" within the part number does not necessarily denote "automotive specifications" ("AEC Q-100"). On some of the older National parts, it can denote Automotive grade, so consult the datasheet.
For native TI devices, "Q" simply denotes the -40°C to 125°C temperature range, just as "I" denotes -40°C to 85°C and "C" denotes 0°C to 70°C.
Automotive specified devices ("AEC Q-100") END with "Q1", regardless of the actual "Q" grade temp range (usually 0, 1, 2 or 3).
I just want to make this clear, as there have been customers that assumed the devices were Automotive grade because there was a "Q" in the part number.
So the LM2903VQDR is NOT an automotive grade device, but a -40°C to 125°C temp range commercial device.
But the difference between the two devices above is that the "V" LM2903VQDR version is specified to 32V max supply, vs 30V for the non-V LM2903D. Below 30V, they are the same.