This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMH5401: TIA LMH5401 and amplifier (2 steps)

Part Number: LMH5401

Hi!

We need to do a TIA for space application. The first step is done with a commercial amplifier (LMH5401). For that, I use two; one of this is used like TIA (with input +-5uA with 400MHz) and the output is more or less +-2.6mV according to simulation (I saw it in this forum). The second step is amplifier that output, but I only see +-60mV. What is the maximum amplitude in Vout for this application? It is possible to reach Vout about 1.5V of amplitude? The circuit simulation is:

Thank you in advance.