Part Number: TLV9054
Hi Team,
My customer wants to know the background (2) note in "Absolute Maximum Ratings".
They argues that (1) and (2) are contradictory if (1) violation under regulated less than 10mA could affect device life reliability.
Could you tell me what is the intention of the Note (2) in "Absolute Maximum Ratings"? I thought that this intended that the power rating of the ESD Diode built into the V⁺ from the Signal Input pin is 0.005W (0.5V*10mA), is that wrong?
My customer's design review has been stopped due to the reason we discussed that in the following E2E thread. And I need to explain the background in meeting with them
Regards,
Takashi Onawa