This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM358: Using LM358 as a replacement to LMV324D

Part Number: LM358
Other Parts Discussed in Thread: LM324, LMV324, LT1013

Below is a project I am working on using op amp to amplify input to a range of 15 V for the PWM output. Original design was utilizing LMV324D but now we intend to use LM358D.

On the second schematic, it is showing the power supply circuitry to both op-amp and from it you should expect 15 V being supplied to the Op-Amp but instead we are getting only supply voltage of ~2.5 V. Now when the R79, R80, R81, and Z2 are removed, the Op-Amp seems to be working fine. The original design using the LMV324D(with different power supply voltage) worked fine.

My issue here is why does the power supply drop to 2.5 V with the inclusion of the R79, R80, R81, and Z2.