Part Number: TL082
Hello Team,
- Can you confirm that the TL082 has input ESD diode?
- What is the maximum current they can withstand?
The TL082H is well specified and says that the inputs have ESD and can withstand 10mA, so you can get over voltage situation on it by limiting the current.
The details are on table 6.1 note 3.
- Specifically, on the TL082 if I have Vin 15V with 1Mhom limiting the current down to 15uA, would it be a problem for the ESD diode?
The over voltage situation can remain for long time >seconds +.
Thanks,
SunSet