Other Parts Discussed in Thread: MOTORWARE, DRV8305
Hi,
I'm running a BLDC motor using Motorware FOC lab05b, my motor is 57HBL74, see link below for details.
We are moving a load up and down via a lead screw and some gearing.
The load is up to 200 kg moving at about 25 mm/sec on the up stroke.
At about 120 kg things works just fine, up and down. The speed is controlled by the PID controller nicely.
With 200 kg load on the downs stroke when the gravity is helping the motor the software fails (and never recovers) and the load basically freefalls.
I just noticed this so I've not yet hooked the BOOSTXL board to Code Composer Studio debugger to see what actually happens,
that will have to wait until Monday but I figured I'll put the question up here what could be the problem so I can use the weekend to mull over the possibilities.
Have a nice weekend everyone,
wbr Kusti