Hi,
In a xx_algPlugin.c, a AlgorithmLink_xxProcess function receives 'inputBufList' as a input parameter.
A value of inputBufList.numBuf means a number of buffers.
For example, in my case, this value comes to 4.
How can I change this value to 2 and which part of source code involved for that?
I set a input channel number to 2 for dual camera capture actually.
So, 4 buffers are filled with channel index [0],[1],[0] and [1].
Does it means that a first index[0] buffer and second index[0] buffer is sequencial?
I need only one frame per each channel.
How can I get this?
Thank you.