Tool/software: Linux
Hi Sitara support Team,
My customer is facing that the Ethernet the mass-produced AM3352 board can not be connected.
Here are the status.
-When it operates continuously, the initialized network setting is occurred very rarely.
-From the following kernel message, it seems to operate again that the processing should do only at the power on.
*Linux kernel message*
[20.831927] net eth0: initializing cpsw version 1.12 (0)
[20.883872] net eth0: initialized cpsw ale version 1.4
[20.942486] net eth0: ALE Table size 1024
[21.086731] SMSC LAN8710/LAN8720 4a101000.mdio:00: attached PHY driver
[SMSC LAN8710/LAN8720] (mii_bus:phy_addr=4a101000.mdio:00, irq=-1)
[21.153309] libphy: PHY 4a101000.mdio:01 not found
[21.183308] net eth0: phy "4a101000.mdio:01" not found on slave 1, err -19
[21.292622] IPv6: ADDRCONF(NETDEV_UP): eth0: link is not ready
[23.206769] cpsw 4a100000.ethernet eth0: Link is Up - 100Mbps/Full - flow control off
[23.214724] IPv6: ADDRCONF(NETDEV_CHANGE): eth0: link becomes ready
-PHY device: LAN8710
-CPU, OS information;
Linux version 4.9.28-geed43d1050 (Custom@ubuntu) (gcc version 6.2.1
20161016 (Linaro GCC 6.2-2016.11) ) #1 PREEMPT Thu Jul 27 10:21:18 JST 2017
CPU: ARMv7 Processor [413fc082] revision 2 (ARMv7), cr=10c5387d
OF: fdt:Machine model: TI AM335x [Custom info]
[Question]
1. Could you please provide me the way of verification?
2. Was there similar report so far?
I will post the other information such as the frequency of connection error, the boot log,
their file system after getting the reply from my customer.
Best regards,
Kanae