This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
Our customer had proceeded to build ES unit and measured noise floor of PCM4202.
Then low frequency 20Hz noise floor level is 15dB higher from 1KHz.
And also Vcom noise characteristics has almost same low frequency noise.
It seems ADC output noise floor got strong influence from Vcom noise.
They want to verify this characteristics on PCM4202EVM but we can not find EVM here.
Could you duplicate it on your site.
I will forward you our customer captured noise floor data to your private mail box later on.
Regards,
Mochizuki
Hello,
Here is additional information from the customer.
Their input buffer stage is not OPA1632 type differential amp but normal OPAs are used for non-inviting and inverting stage biased by VCOM.
That is why VCOM noise is not canceled.
Can we take a workaround that filtering VCOM noise by RC filter from VCOM pin to OPAs? Do you see any concern?
Regards,
Mochizuki
Hi Mochizuki,
It's always recommended to have at least 0.1uF bypass capacitance on VCOM. Are you sure they are not testing with the HPF of PCM4202 disabled? Are they measuring VCOM noise at the VCOM output, or at the output of their amplifier? It may also be possible that the amplifier is contributing significant 1/f noise.
Best,
Zak