Hi,
We have designed a board with one ADC(PCM4202) and DAC, both are working at 96KHz of fsample and MCLK of 24.576 MHz (256fs), but each one working with different clock, I mean, they are not synchronous each other. In these conditions the DAC's clock leak to ADC input because we can see very noise in ADC spectrum. What are the points more sensitive in the PCM4202 to this clock?
We have tested to make to work the ADC and DAC with the same clock (synchronized each other) and we don’t found this problem. In our application, these clocks have to working in asynchronous mode. Thanks.