Hello,
Can we get DSP mode LRCK (Frame sync) output in Master mode?
At Table 37. Page 0: Register 11 Field Descriptions
Bit4 shows
0: duty cycle of LRCK is 50% (default)
1: duty cycle of LRCK is 1/256 (similar DSP mode)
But we cannot have 1/256 Frame sync output.
The other hand, at Figure 46. Audio Format for TDM
There is comment as below.
50% Duty Cycle (Master Mode)
1BCK or 50% Duty Cycle (Slave Mode)
It is just confirmation, which is correct?
Regards,
Mochizuki