Other Parts Discussed in Thread: PCM9211
Hi,
I hope someone can help me and save me some time.
I am using a PCM5121 in a design (well 5 of them actually) and I just need to know which registers needs setting and their values for the chip(s) to act as simple D/A converters.
I am supplying a basic I2S signal set at 192 kHz sampling rate to the input pins BCLK, LRCLK and DIN and this signal is a -10 dBFS sine wave at 1 kHz
The XSMT pin is pulled up to VDD so the soft-mute should not be engaged
I have an IIC interface connected and I can read/write the internal registers...
_BUT_
I am not getting any audio output from pins 6 or 7
We are not supplying a signal to SCLK so...
I have set register 0x0d to 0x10 to tell it BCLK is the reference for the PLL (register 0x04 tells me that the PLL is locked)
I have set register 0x0e to 0x40 to tell it BCLK is the reference for the D/A converter
Can you please tell me if there is something obvious that I have missed to get audio out of this device
thank you for your time
kind regards
PhilipJ