Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed from November 25 through December 2. Thank you for your patience.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TAS5634EVM: Is it possible to play more than 20Khz?

Part Number: TAS5634EVM
Other Parts Discussed in Thread: DIX4192, TAS5634, TAS5558

Is it possible to play more than 20Khz with EVM? (i.e. 30kHz~40kHz)
In case of USB input, it is transmitted to the load by TAS1020B --> DIX4192 --> TAS5558-->TAS5634, and I checked the Max Sampling rate of each IC is almost 200kHz.
When I actually test it, it does not play at 20kHz or higher.

In case of the optical input it does not work.
Can it be solved through register setting of TAS5558 audio processor?