Other Parts Discussed in Thread: TPA3255
Curiosity question related to the TPA3255 EVM Schematic, I noticed that on VDD a 10uH inductor was used but on GVDD_AB and GVDD _CD no inductors are used, is there a reason for this? They do have zero-ohm resistors there like they may have tried it but not used them on the final product. Did they try inductors there and it didn’t help anything or where these used for something else? If the original people that did the work are no longer at TI don’t waste time on this answer.