Hi TI experts,
I have came across a problem when using TAS2110 AMP IC for my design, which i am not able to obtain the output power (6.1W) as mentioned in the datasheet.
I only manage to get around 2.25W (3Vrms)
My measurement condition is as below:-
TAS2110 Input signal : -6dBFS (by APx525 machine)
Speaker impedance : 4Ohm
Internal booster : Yes
Boost mode : multilevel boost
Internal boosted voltage : 12V
Amplifier gain : 16dBV
Volume gain : 0dB
Please teach me how to get the output power (1%) - 6.1W by using above setting.
Thank you.