Other Parts Discussed in Thread: TAS2110, TAS2564
I've been using TAS2110 in my design for a while. It works fine. Last year it became unavailable, so my product upgraded to TAS2563, which seems to by pretty compatible with the former one. Unfortunately, new boards don't work properly. The sound is correct, but occasionally a buzzing is heard together with the sound.
Most settings are default. Working parameters are: 22,222 ksamples/s, 16bits/sample, 2 time slots. That gives SBCLK/FSYNC=32. Chapter 8.4.2 of Data sheet doesn't indicate this as allowed value, however it is supported by PPC3 software. I use AUTO_RATE detection and TDM_DET register reports proper value (0x02). No errors are reported.
Are there any special setting or conditions required by TAS2563 to work properly?
Regards