Hi Expert,
when I use the PCM5121 GDE GUI to configure the Biquad, I found strange issue when I add high frequency EQ point.
1. EQ setting 1000Hz,10dB,Q=2, I can get the expected Graph as below.
2. when change the EQ frequency to 10Khz or even higher , the full band gain is dropped, this is not expected. and customer's test data is matching the PPS Graph showed result. but why?
Please help me to fix this or explain the reason.
thanks.
Anderson