This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM1972: 60dB analog gain control

Part Number: LM1972

Hi team,

I'm looking for a solution that enables analog gain control with 60dB attenuation.

I see an application note below, like it but need more attenuation. DC voltage is preferred as control way than serial interface (ex:I2C) since a potentiometer is used with knob. 

https://www.ti.com/lit/ug/tidu034/tidu034.pdf

Can you suggest recommended solution?

Best regards,

Hayashi

  • Hi Hayashi-san,

    Have you considered to adjust R8 and R9 from the same reference design to change the gain of the circuit? You may recreate the same simulation on TINA or PSpice .
    The integrated volume control devices have all digital control.

    Best regards,
    -Ivan Salazar
    Applications Engineer