Hi
We would like to confirm / check do we need to disable the DRC feature in the AIC3254 initial sequence (if we don't require the DRC feature).
Currently, we used the PRB_P2 (Page 0 / Register 60: 0x2).
Thanks
BR
Trevor
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
We would like to confirm / check do we need to disable the DRC feature in the AIC3254 initial sequence (if we don't require the DRC feature).
Currently, we used the PRB_P2 (Page 0 / Register 60: 0x2).
Thanks
BR
Trevor
Hi pdjuandi,
Thanks for your reply.
Add more questions, if we don't need the DRC function.
For PRB_P2, we need to disable the DRC function in initial stage.
For PRB_P3 we don't need to disable the DRC function in initial stage.
Is the above correct?
BR
Trevor
If you don't need DRC, then use block without DRC like PRB_P3 and power consumption is lower than PRB_P2.
Example see section 2.5.0.3.2.