Other Parts Discussed in Thread: PCMD3140
Hello team,
I’d like to check if PCM6480-Q1 is compatible with A2B interface. Would you please answer the followings?
-. For PDMDIN/CLK pins, is it capable of interfacing with A2B format which is output from DMIC (with A2B IC)?
-. If it’s possible, all four DMICs can be connected to one channel of either PDMDIN1/CLK1 or PDMDIN2/CLK2?
-. For TDM output pins, can the A2B data send to the audio Amp? Is the A2B data compatible with TDM format?
-. So, can PCM6480-Q1 support the following configuration?
: G-sensors and DMICs -> A2B format -> PCM6840-Q1 -> A2B format -> Audio Amp
Thanks,
Sam Lee