This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TAS5710: Effection of power supply

Part Number: TAS5710

Hi team,

My customer would like to use this device, but has one concern with it.

They will put 12V to AVCC, and worrying about the effection of the noise in the power supply

In the datasheet, it says that this device has an internal regulator. So, with the high PSRR of the internal regulator, the effect on the power supply noise is very low.

Is it the figure1 characteristics that the customer should look up?

Also, can you provide the internal block diagram of this device? (including the internal regulator)

Regards,

Ohashi