It found that the output overcurrent protection when TPA3116D2 in master/slave synchronous operation, caused the output power decline in100HZ.
If the IC works separately are normal. It also works stably above 1KHZ. If the master SYNC pin connect a 10K resistors to GND, the output inductance heats very badly.