This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TAS2X63EVM: How to use PP-SALB2-EVM with TAS2x63EVM?

Part Number: TAS2X63EVM
Other Parts Discussed in Thread: PP-SALB2-EVM, PCM9211

Hi team,

Q1. If I want to evaluate Tas2x63EVM with optical inputs, Can I use the PP-SALB2-EVM LearningBoard 2 to do so? 

If yes, Would you check if below configuration is right method?

  • Vbat=5V
  • PVDD=11V(external PVDD used)
  • 8Ohm load(dummy connected to AP)

Q2. If I connect learning board to TAS2x64EVM, Does XMOS automatically select I2S signal path from MUX? 

Thanks

Jay.