I have connected a TLV320ADC3101EVM-K via USB to a PC and it is not being detected by the ADC3101 CS software. Here's a screenshot:

In Device Manager, the eval board shows up like this:

I have installed and re-installed the ADC3101 SW twice with the same result. The last time as an administrator. This PC is Win 10 64-bit. I have set all of the default switch and jumper settings as described in the eval board manual.

What else should I try to get this eval board detected properly by the ADC3101 software? Thanks.