This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV5825P: DRV5825 voltage issues

Part Number: DRV5825P

help~

The voltage of the DRV5825 board we designed ourselves cannot reach above 10V. After increasing by 10V, the DRV5825 cannot function properly. The register status register displays 0x16 (indicating that it is being reset), but it is not faulty when using our main control to connect to the official development board. The hardware principle is completely consistent with the chip manual, and now it is somewhat confusing. We hope to seek technical support

DRV5825 我们自己设计的板子 电压 无法上10V以上,上升10V以后 DRV5825 无法正常工作 寄存器 状态寄存器显示0x16(提示正在复位)  但是用我们的主控接官方开发板却没毛病  硬件原理方面 完全和芯片手册保持一致 现在有些摸不着头脑 希望寻求一下技术支持