I'm confused by the datasheet.
For VinL and VinR it states an absolute max rating of –0.3 to (VCC + 0.3 V) < 6.5
These inputs are AC coupled though so are these the maximum values with the internal bias applied? or is it just the peak-to-peak voltage range?,
Also in section ANALOG INPUTS TO ADC it says "These are single-ended (unbalanced) inputs,
each capable of 0.6-VCC Vpp input with 10-kΩ input resistance, typically." Let's assume Vcc is 5V, does this mean 4.4 Vpp is allowed?
Best