This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SRC4392: Multiple SRC4392 DIT Output Sync

Part Number: SRC4392

We are designing a board using 4 x SRC4392, all as both DIR and DIT. We would like to make sure the DIT outputs of all 4 devices are synchronised (the source data will have the same MCLK, BCLK, LRCLK).

From the datasheet it looks like the way to do this is to set the first SRC4392 device to output on the BLS pin, then connect that to the other 3 SRC4392 devices with BLS set to an input.

Is this correct? And if so, am I also correct that the SYNC output pin isn't needed for this? (in which case I'm not sure I understand why that's there)