Dears,
Customer have some questions as follow:
1.Does PCM2900C need a drive to operation and can support android linux system or not?
2.The chip supports USB input and analog input,how to switch the two input?
Thanks
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Dears,
Customer have some questions as follow:
1.Does PCM2900C need a drive to operation and can support android linux system or not?
2.The chip supports USB input and analog input,how to switch the two input?
Thanks
Hi Ning,
1. PCM2900C is USB class compliant. No driver is required. I'm not super familiar with Android Linux, but if it supports the USB class, then it will support the device
2. I don't understand what you mean by "switch the two input." The two inputs are independent of one another. The analog input is for the recording path and the USB input is for the playback path.
Best regards,
Jeff McPherson