Dear TI experts,
Last time I requested a review of the schematic of my customer.
they tested 1st sample, and they found that there is a pop noise when the power is off.
and they fond a way to remove it.
they remove C61, and pop noise disappeared.
1. Is it okay to remove C61?
2. in EVM, there are no other components even resistor, but in the datasheet, there is 100Kohm pulldown resistor for MUTE pin.
Is it okay to remove R68 resistor like EVM? or is it nessary? what is the recommended value? 220ohm or 100Kohm?
Best regards,
Chase