This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi TI Support Team,
I have tried three different AC5140EVM boards and still cannot connect the EVM board. The PPC3 has used the latest version V3.2.1
The hardware configuration and setting below, Both USB and ADC green LED are lighted, However, the PC is not able to recognize the EVM board. nothing has changed on the device manager, and the USB-ready Blue LED is not lit.
P.S. We already installed three PCs and also the same issue. Please help us. Thanks!
Regards
Kelvin Lo
Hi Kelvin,
Please check in device manager for the PC's USB connection to the EVM, sometimes monitors or additional systems can interfere with the connection.
Regards,