Other Parts Discussed in Thread: TAS6424LS-Q1
Hello, I'm using the TAS6424LS-Q1 IC for vehicle project.
In my test pre-condition is below.
BTL mode
Input audio : 0dB
AMP setting : 0dB volue, 15V peak output voltage
In this situation, I use the PVDD with 15.5V and the clip detection is not detected for connected 1 channel speaker(4ohm).
But the PVDD with 14.4V, the clip detection is detected. I think that this detection is alright. Is it okay?
Additionl, I ask that if the case of PVDD with 15.5V in not clip detection environment (only 1 channel), if the speaker additional connection for 4channel, it will be effect to clip detection?
Please reply my question, Thank you.
Best regards,