Other Parts Discussed in Thread: TAS2563,
Problem:
Settings are written to the EVM, but no audio is heard in USB playback.
Additional observations:
- Plugin TAS2563QFN is used (problem is the same with TAS2563 plugin).
- In the PPC Audio Player it is not possible to set the USB device as suggested in 'slou408.dpf'), but the EVM is chosen as default speaker in Windows and volume control is at 100%.
- Background hiss is audible in speaker (very low level).
- I2S signals (EVM testpoints) are active: 1.8V logic, SBCLK is 12.3MHz, FSYNC is 48kHz, SDIN is 24 bits.
- TAS2563 speaker output PWM is active, switching spikes every 2.5us (400kHz), spike length 100 to 300ns.
Hardware:
TAS2X63EVM (default jumper settings), USB connected, VBAT/GND 5V supply (4V also tested), speaker is connected to Out+/Out-).
PVDD has no external supply (voltage is same as VBAT supply). D4 is present on the board.
J27 and J29 are set to USB(int)
J18 is set to 1.8V
J3 is set to 3.3V
J24 is set to I2C
J14 is set to SS0
J22 and J23 are connected
Software:
PurePath Console v3.2.1
FW version 1.1.0.0
Plugin TAS2563QFN v.3.0.0
PC:
Default PC speaker is 'TI USB Audio UAC2.0'
Audio Device Control Panel is set to '8 channels, 24 bits'
Speaker sampling rate is set to '24 bit, 48000 Hz'
PC OS is Win10E