Other Parts Discussed in Thread: PCM5242, , , TPA6130A2, TLV320AIC3105, PCM4104, TAC5212
Hello,
I have a PCM5242 DAC in which I would like to control two separate line-level (2VRMS) outputs with discrete volume controls for each output. I would like to control the volume of each stereo output pair using I2C control. Can I use two TPA6140A2 units to add analog volume control to those two separate outputs (with an I2C multiplexor so I can control each separately)?
What will the total VRMS output of the TPA6140A2 be? Would it be "too hot" to drive a standard 10k input pin on a consumer device for example? Is there a way that I can keep the TPA6140A2 volumes low so that it doesn't overload the inputs on the receiving device?
The TPA6140A2 has a "tapered volume" control which is nice. But that means that I really shouldn't just "limit" in software the maximum height of the volume level, because I would then lose the tapered control benefits. So I guess I would have to turn the gain down sufficiently so that at 100% volume, the TPA6140A2 is only driving 2VRMS out, to not overload the input on the receiving device.
Any ideas on this? Are there any other products that would work as a line driver with I2C volume control in the sub $1 range?
Thank you,
Jay