Hi,
We are developing custom board for one of our client(Audio application).We are using TPA3110D2PWPR Audio amplifier to connect with two 10W speaker.
Below is the issue which we are getting when we powerup the board and send the audio signal to amplifier input.
1.SD and fault pin has been shorted and given pullup resistor.But Amplifier is pulling it low through fault pin and the cause is unknown.There is no thermal issues and no short on input capacitors.But we are suspecting DC detect.so we removed the output filter inductors and input capacitors also done the power cycling but still we are not able to isolate the issue.Let us know how to get fault pin back to high state.