Loading filter coefficients from Pure Path into a TLV320AIC3120EVM-U via USB from a Windows PC. (Download and Run in the Build menu). The module, which was passing audio at the time, stopped communicating with the PC and the yellow indicator on the module went off. PC now reports Unknown USB device (Device Descriptor Request Failed).
The evaluation module was working perfectly prior to this happening. Only anomaly was on a previous Download and Run it threw up a request to update the firmware on the module to correct an audio level problem. This update failed but the module was still working after the update failure. For this subsequent download I declined the firmware update.
I tried a different PC with a fresh installation of Codec Control. Same problem.
Power supply voltages on the module are OK.
Any suggestions ?