Other Parts Discussed in Thread: TAS5827, TAS5805MEVM
Dear Sirs and Madams,
We are verifying the I2C communication of TAS5825.
Page 42 of the datasheet describes "9.5.3.1 Startup Procedures", but I would like to confirm two points.
1. Is it correct that I2C communication becomes valid 5ms after *PDN is asserted to High?
2. Is it correct to think that I2C and I2S are independent?
I understand that "9.5.3.1 Startup Procedures" is just the I2S operation start sequence, and that I2C commands can communicate 5ms after *PDN goes High, as shown in red in the figure below. Is this recognition correct?
/* TAS5825M datasheet URL */
Regards,
MM