Hi team,
The customer was always accused of having a low output volume during testing, and then adjusted the DSP output to a very high volume. After the adjustment, the AMP kept reporting a 0x24->01 (Clip Warning Register) warning. I would like to know what impact this warning will have if it continues to exist. ?
My analysis:
Regarding the issue of low volume, I think it is necessary to check whether the customer's Gainlevel setting is close to the input voltage of TAS6424E-Q1. I will confirm with the customer later.
But after the customer adjusts the output audio of the DSP, why does the clipping problem occur? How should I analyze this problem?
If the problem of clipping occurs, will it affect the normal operation of the circuit after clearing the clear fault at 0x21 bit 7?