This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Dear Designer,
The jumper and MIC configuration voltages have been adjusted to the configuration, but when the headset is plugged in, it is the computer that is heard, not the MIC pick-up. What is it?
Thank you very much!
Best Regards,
Arabella Zhang
Hi,
Are you executing the script like the one shown below from the GUI for recording?
This script is just for recording, it does not include the playback to headset.
If you need it to playback to headset, you will need to add that in the script and externally loop the data out DOUT back to DIN.
Regards.
Hi pdjuandi,
I asked the customer to organize the problem into a document. Could you please help me find out the specific reason?
Functional requirements: Collect audio from MIC, and output MIC audio signals from HPL and HPR lines, that is, MIC input and headphone output.
Problem: Currently, the MIC audio collection and headphone line output verification functions cannot be configured.
Thank you very much!
Best Regards,
Arabella Zhang
Hi Arabella,
Please get more information about their testing. Have they tried my suggestion above, are they using the scripts from the GUI etc.?
If they are using the EVM, they can quickly run the following steps to verify the recording and playback.
Steps to record with the recording script above:
Steps to hear the playback tone:
Once the above steps are confirmed working, then combine both scripts and connect DOUT to DIN so they can play sound on MIC input and listen through HP/LINEOUT.
Regards.