Hello,
My question is related to the followings, but the 2nd one isn't available now, so please let me ask you a few questions.
https://e2e.ti.com/support/data_converters/audio_converters/f/64/p/403678/1432310#1432310 <= The link isn't available now.
I understand the RC on the input pins(VINL/VINR) shown in figure24 on page 17 in the datasheet is for HPF as the note.A says. I also do that there is an internal HPF which can be bypassed(BYPAS=high) or used(BYPAS=low). The cutoff frequency is different between those, but both work as HPF.
1. Would you please tell me if the input filters for VINL/VINR pins are really mandatory since 8.2.2.3 on page 18 says "AC coupling capacitor muse be placed in series with the input"? If yes, would you please tell me why it is because it has internal HPF instead which can be configured by BYPAS=low?
2. Would you please tell me what would happen if the external RC filter isn't used, but only the internal HPF by BYPAS=low is done?
3. If my customer can use BYPAS=low without doing the external RC, is the following all they have to check for the VINL/VINR pins?
4. Would you please tell me the differences between using the external R1/C1/R2/C2 and using internal HPF by BYPAS pin(#8)=low? I know the Fc is different, but I'm not sure other than that.
Best Regards,
Yoshikazu Kawasaki