I have designed in the TAS5431QPWPRQ1 to drive a speaker which DRC is 4Ω. When I power on the circuit, the TAS5431-Q1 can not work . I can read the Fault Register
(0x01) is 0x08. Then I changed the load to 16Ω,but it stil remind 0x08. I'm sure the output didn't short. Could you help me to analyse this problem? Thank you.