Hi,
I have tried different sample codes from the forum and the internet but have not been able to get any output from the speaker.
Following are the commands i have prepared and correlated with the datasheet, all I2C commands execute fine and confirm the writes by readback.
Following are the sequence of write performed.
// Clock-gen muxing. PLL_CLKIN=MCLK, CODEC_CLKIN=PLL_CLK 12.288MHZ // P=1, R=1, J=6, D=10000, // NDAC=NADC=7, MDAC=MADC=3, // DOSR=AOSR=384 => 16KHz fs static const tlv_cmd_t init_cmd[] = { {0x00, 0x00}, // Page 0 {0x01, 0x01}, // sw reset // PLL config {0x04, 0x03}, // Clock-gen Mux. PLL_CLKIN=MCLK, CODEC_CLKIN=PLL_CLK {0x05, 0x91}, // PLL P+R. PLL power up, P=1, R=1 (P=divider,R=multiplier) {0x06, 0x06}, // PLL J = 6 {0x07, 0x27}, // PLL D fractional. D-value MSB = 0x27 {0x08, 0x10}, // PLL D fractional. D-value LSB = 0x10 // mode master {0x1B, 0x0C}, // mode is i2s master, wordlength is 16, BCLK/WCLK out // divider configs {0x0B, 0x87}, // NDAC is powered up and set to 7 {0x0C, 0x82}, // MDAC is powered up and set to 2 {0x0D, 0x01}, // DOSR = 384 0x180, DOSR(9:8) = 0x01 {0x0E, 0x80}, // DOSR = 384 0x180, DOSR(7:0) = 0x80 {0x12, 0x00}, // NADC divider is powered down and ADC_DSP_CLK = DAC_DSP_CLK. {0x13, 0x00}, // MADC divider is powered down and ADC_MOD_CLK = DAC_MOD_CLK. {0x14, 0x00}, // AOSR = 256 0x100, AOSR(7:0) = 0 // {0x74, 0x00}, // DAC => volume control thru pin disable {0x44, 0x00}, // DAC => drc disable, th and hy {0x41, 0x00}, // DAC => 0 db gain left // {0x00, 0x01}, // Page 1 {0x21, 0x4E}, // De-pop, Power on = 800 ms, Step time = 4 ms {0x1F, 0x84}, // HPL {0x23, 0x40}, // LDAC routed to HPL {0x28, 0x0E}, // HPL unmute and gain 1dB {0x24, 0x00}, // No attenuation on HP {0x25, 0x00}, {0x2E, 0x0A}, // MIC BIAS = 2.5v {0x30, 0x40}, // MICPGA P = MIC M 10K {0x31, 0x10}, // MICPGA N = MIC N 10K // {0x00, 0x00}, // Page 0 {0x3C, 0x0B}, // select DAC DSP mode 11 & enable adaptive filter // {0x00, 0x08}, {0x01, 0x04}, // {0x00, 0x00}, {0x3F, 0x96}, // POWERUP DAC (soft step disable) {0x40, 0x04}, // Unmute DAC {0x51, 0x80}, // Powerup ADC channel {0x52, 0x00}, // Unmute ADC channel // {0x00, 0x01}, {0x2A, 0x1C}, // Unmute Class-D left {0x20, 0xC6}, // Power-up Class-D drivers }; static const tlv_cmd_t loop_back_cmd[] = { {0x00, 0x00}, // Page 0 {0x1d, 0x1d}, // b4 = ADC-to-DAC loopback enabled {0x00, 0x01}, {0x2e, 0x0a}, // MICBIAS = 2.5V {0x26, 0x4c}, }; static const tlv_cmd_t beep_cmd[] = { {0x00, 0x00}, // Page 0 {0x40, 0x0C}, // mute DACs {0x0B, 0x07}, // power down NDAC divider {0x47, 0x80}, // enable beep generator with left channel volume = 0dB {0x49, 0x00}, // BeepLen HIGH {0x4A, 0x7D}, // BeepLen MID {0x4B, 0xA0}, // BeepLen LOW {0x4C, 0x59}, // BeepSin MSB {0x4D, 0x98}, // BeepSin LSB {0x4E, 0x59}, // BeepCos MSB {0x4F, 0x98}, // BeepCos LSB {0x0B, 0x87}, // NDAC is powered up and set to 7 {0x40, 0x04}, // Unmute DAC };
Following is the circuit diagram
.
Following is the PLL calculation