This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi!
I'm trying to debug a system based on a TAS5713 and a LM3S9B96, I've finally got the processor to output some I2S-data but I dont get any switching on the output of the amp. The amp is configured for BD-mode, and ASEL_FAULT as output. Fault isn't indicated but when I poll (after writing error reg with 0x00) I get different answers in a sequence:
Error: ff
Error: 30
Error: 30
Error: 30
Error: 30
Error: ff
Error: f0
Error: 97
Error: 01
Error: b8
...
I'm just polling the register a couple of times, and its the same sequence after a restart.
Any ideas? =)
Additional information:
I get this "error sequence" in both running and shutdown mode. The amp asserts FAULT low directly at exit shutdown, the supply voltage is 12V and there is a resistive dummy load at the output.
I've noticed that there is a small peak at the output every 1s when in run-mode (not switching), could this be some sort Overcurrent thats kicking in?
Hello Erik:
Did you do an oscillator trim? What is your initialization sequence? Please also make sure that the I2S clocks are stable.
Best regards,
Tuan
Hi!
Yes the oscillator trim should be done, and the clocks seems to be stable.
My initialization sequence is (pseudo code):
Drive PDN High
Wait 1ms
Drive RESET high
Wait 14ms
Run Oscillator Trim
Wait 50ms
Configure ASEL as Fault
Configure ICD Registers for BD Modulation
Configure mux Register for BD Modulation
Exit shutdown
Wait 200ms
Replaced the board and now It starts switching atleast. But the switching frequency isn't properly filtered out, there is a 4Vpp ripple on the output (I'm using 10uH inductors and 680nF capacitors)
The polling error reg answers is still the same even though it now is running.
Hello Erik:
I am not sure if you clear out the error register by writing 0 before you read it back.
What is your PVDD level and your load impedance?
Thanks,
Tuan
Yes, the register is written with 0.
PVDD is 12V and the impedance is close to 8Ohms
After a while I realized that I was using a AD-filter for the BD-modulation, information about the output filter in the datasheet maybe would be smart?
Well, soldered in the SSTIMER cap and use the amp successfully in AD-mode...
But still the main question remain, why does the error reg register errors when its running succesfully?
Hello Erik:
The TAS5713 is in an autodetect mode, meaning when the I2S clocks are good, it will run. It won't report any faults unless there are some glitches in the clock or the ratio between Fs/MCLK and/or Fs/SCLK are not correct. So when you clear the faults and then if the glitches are there, it will report again. If you run sine wave through, do you see any discontinuity?
Best regards,
Tuan
Hi again!
The thing is that it seems to be working just fine, I get a glitch free sinewave, but when I poll the error-register it indicates an error, and as you can se the response isn't consistent.
I'll try to check my code again.
Greets, Erik