Tool/software:
Hello E2E,
I have a circuit where PCM is receiving (BCK, LRCK and DIN) on its AUXIN0 port and SPDIF output is connected to MPO0.
So far i have setup the registers correctly the best of my knowledge but there is no sound on soundbar.
I have tried generating a script from EVM codec control software but i could not setup DIT to receive data from AUXIN0.
Here are the configurations that i have performed.
REG -> Value
0x60 33h
0x78 DDh
With the configuration mentioned above there was no signal on MPO0 so i researched and found that i had to provide MCK to DIT, since there was no MCK on input side i routed the XTI from ADC to the DIT as such
0x60 23h
I started receiving output on MPO0 but still no audio on soundbar.
Can someone point out what im missing or where im messing up please
Here are the schematic of my project
Thank you