This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TAD5212: Low group delay devices

Part Number: TAD5212


Tool/software:

Hi team,

I didn't get a response so I'm reposting.
Is there a DAC with low filter group delay?
I am looking for a device with less group delay than the TAD5212 as a standard.
I would appreciate it if you could introduce me to some of them.

Sincerely,
Ryu

  • Hello Ryu,

    the group delay of all our DACs are mostly mentioned under  filter's   delay and it is related to sampling freq ( so it changes for a given device based on sampling frequency.)

    Some devices such as PCM510x family have normal and low latency mode which gives you a different option, For this device for example, normal delay of 20/Fs  changes to 3.5/Fs for low latency mode. Some of our DACs have a fixed delay ( such as PCM178x or 270x families which have fixed  delay of  20/Fs). Some devices such as PCM512x and PCM524x family have several option for filter selection and thus have  more option for delay time . In this case you can select from  1.2/Fs , 3.5/Fs, 20/Fs or even 33.7/Fs.

    I believe  PCM512x and PCM524x families offer the lowest group delay with high performance as well.

    Regards,

    Arash

  • Hi Arash,

    Thanks for the reply.
    I understand about the product.

    Sincerely,
    Ryu